Interface’s 1200 Standard High Capacity Load Cell can be attached in between the hydraulic jack and a heavy load. The 1200 Standard High Capacity Load Cell will measure the forces of the hydraulic jack as it lifts the load cell located in between the jack and the object. With the 9890 Strain Gage, Load Cell, & mV/V Indicator, the customer is also able to see the results in real-time.